News Release Archives
Note that the releases are accurate at the time of publication but may be subject to change without notice.
Research & Development
2012
- Jun 20, 2012
- Mitsubishi Electric Develops High-output, High-efficiency GaN Power Amplifier on Si Substrate for Mobile Communications Base Stations
- May 23, 2012
- Mitsubishi Electric Develops All-SiC Inverter with High Power Density
- Apr 25, 2012
- Mitsubishi Electric Develops 14GHz Power Amplifier with World's Highest Output Power for Satellite Communications
- Mar 8, 2012
- Mitsubishi Electric Develops EV Motor System with Built-in Silicon Carbide Inverter
- Feb 7, 2012
- Mitsubishi Electric Develops Multi-Band Power Amplifier for Automatic Band Switching and Seamless Roaming