Factory Automation

Human Machine Interfaces MELHMI-GOT MELSOFT GT Works3

MELSOFT GT Works3

Professional designs. Maximized efficiency. Intuitive operations.
All made possible by GT Works3.

This integrated software is used to create professional screen designs for GOTs. Developed with the concepts of simplicity, sleekness, and userfriendliness in mind, this is a powerful tool that pushes boundaries and delivers endless design possibilities.

/.c-list

Engineering with Ease

Engineering with Ease
  • 1 Work Tree

    Manage and configure for each screen, system, and project.

  • 2 Data Browser

    Directly view and edit properties of multiple objects across the entire project.

  • 3 Screen Image List

    View each screen as an image, making screen search simple.

  • 4 Library

    Create professional screens using a wide variety of parts and frame animations.

  • 5 Device Search

    Quickly search for the devices and labels in use.

  • 6 Screen Editor

    Design efficiently with various functions that minimize man-hours in screen creation.

Screen Design

Choose from abundant and beautiful parts

UPDATED Library

  • NEW Many new parts in vector format have been added. Vector parts can be specified in full color, and their quality remains consistent even when zoomed in and out. Additionally, the file size remains small even with large parts.
  • NEW Frame animation is supported, making it easier to convey information. In addition to the frame animations registered in the library, other animation files (PNG, APNG, GIF) can also be imported.

Before Raster format

NEW Vector format

With the vector format, edges are displayed with clean lines regardless of size

With the vector format, edges are displayed with clean lines regardless of size

Examples of new parts

Examples of new parts

Design efficiently with batch editing

UPDATED Data Browser

  • All the settings within the project can be displayed collectively and edited directly. This allows efficient review and modification of data, even if there are many screens or settings.
  • NEW By changing and switching the display items of the data browser using presets, you can design efficiently. For example, you can switch to a screen-specific preset when editing screen settings, and to a text-specific preset when modifying text settings. Users can also create custom presets.
Data Browser

Enhanced copy function

UPDATED Consecutive Copy

  • Multiple figures and objects can be copied at once.
  • When copying, information such as device numbers can be incremented based on the original data, reducing the effort of reconfiguration.

[Increment-Supported Items]

  • Device Number
  • User ID
  • Comment Group No.
  • Move Destination ID
  • Comment No.
  • NEW Array Element Count
Consecutive Copy

Efficient scripting

NEW Subroutine of the Script

A process can be divided into reusable components (subroutines). By using these subroutines, development becomes more efficient.

Script:
A language-type program similar to C language, capable of controlling the display of GOT.

Subroutine of the Script

Debug

Debug from your desk even without GOT unit

UPDATED Simulator (GT Simulator3)

  • Operations of GOT can be simulated on a computer using the simulator (GT Simulator3).
  • By specifying the project of the controller to be integrated in advance in the GOT project, the simulator of the controller (GX Simulator3) will automatically start when you start the GOT simulator (GT Simulator3), allowing you to begin debugging immediately.
Simulator (GT Simulator3)

Reuse

Reuse to reduce design man-hours

Add-on projects (sample screens) ready for immediate use are provided, featuring designs with excellent visibility and usability.

Add-On Project for Connections

Servo amplifier connection (MR-J5-G)

Servo amplifier connection (MR-J5-G)

GOT Drive
Inverter connection (FR-E800-E)

Inverter connection (FR-E800-E)

GOT Drive

Add-On Project for Functions

Web camera (USB connection)

Web camera (USB connection)

  • * For the latest add-on projects, please contact your local sales office.

Reuse the project assets easily

Utilize Data

Existing project data for GOT3000 is reusable on a project or screen basis.

Utilize Data

Management

Manage projects easily

UPDATED Screen Tree

  • It is possible to display a list of created base screens, window screens, and mobile screens, and to create new ones or edit existing ones.
  • NEW Group related screens together to keep the project organized.

Display by screen types

Display by screen types

Display by switching tabs

Display by screen groups

Display by screen groups

Screen Configuration (GOT2000)

Screen Configuration (GOT2000)
Work tree Easily manage project data
GOT Graphic Ver.2 Easily create stylish screens
Simulator Check operations with a single click!
Library Easily create stylish screens
Graphical meter Create stylish, clear meters
Table Easily create tables
Data browser Easily check the settings
Device search Quickly search devices and labels
Screen image list Quickly display screen thumbnails
Utilize data (Screens) Search by keywords and effectively use data