Mitsubishi Electric provides semiconductors/devices including power modules and high power devices that handle the highly efficient control of power, optical devices that deliver the performance required in fiber-optic communication devices, high frequency devices that cover everything from radios and mobile phones to satellite communications, and the line of TFT-LDC modules that improve interfaces for information.
Power Modules
Mitsubishi Electric power modules are manufactured with state-of-the-art technologies that ensure the highest levels of performance and reliability while offering impressive energy savings for the products and systems they're used in. Our line-up of products is extensive, ranging from power modules developed to control high-voltage power generation, industrial manufacturing and railway systems to applications in home products, such as controlling the electricity used by air conditioners, washing machines and refrigerators. To maintain our market-leading position, the company's R&D activities aiming to realize further reductions in power consumption and size are ongoing.
High Power Devices
High power devices contribute to increased efficiency and energy savings by supporting the high voltage, high current and usage environment of rollers in steel works, electric power systems and the subway. From rectifier diodes to a variety of Thyristors and stacks, Mitsubishi Electric offers a broad range of new high power devices.
High Frequency Devices
Mitsubishi Electric has long supported the advancement of wireless communication networks through the development of its high frequency devices. Products manufactured utilizing the latest electronics and other technologies combined with newly developed high-performance materials have kept us in a market leading position. Our range of high frequency devices are contributing to the wireless communications infrastructure, helping achieve more reliable wireless communications such as satellite communications, as well as smaller and more powerful mobile phones, and other high-performance network equipment.
IC, Sensors
Mitsubishi Electric's lineup of power semiconductors include transistor arrays, HVICs (High Voltage IC) and sensors. Using the output from a 3-volt microcomputer, our transistor arrays make possible bufferless direct drive, helping contribute to lighter weight and more compact design in a variety of equipment. An HVIC is a high-voltage IC with various built-in protection functions; it uses input signals from a microcomputer or other device to directly drive gates in power MOSFETs or IGBTs. We also provide pressure sensors for such applications as barometric pressure gauges, as well as acceleration sensors to measure vibration in LCD projectors and industrial equipment.
Optical Devices
Mitsubishi Electric is at the forefront of industry in the development and production of laser diodes and modules, including the latest optical fiber communications for broadband and telecommunications networks, and laser diodes for display and industrial applications. Renowned for energy savings, reliability and high performance, our advanced technologies and products can be found in use in major systems for the optical communications infrastructure, as well as in as applications for fiber-to-the-home (FTTH).
TFT-LCDs
Mitsubishi Electric's thin-film-transistor liquid-crystal display (TFT-LCD) modules are built for a wide variety of industrial uses, such as for measuring instruments, automatic teller machines (ATM), point of sale terminals (POS), factory automation equipment (FA) and more. Designed for high reliability, optimal visibility, and enhanced viewability, Mitsubishi Electric's leading-edge TFT-LCD modules ensure optimum performance and excellent color quality in a broad range of indoor and outdoor operating environments. The technologies behind them bring us one step closer to the realization of true images with realistic color and clear visibility in sunlight.
Electronic Devices
Contact Image Sensors that incorporate Mitsubishi Electric’s key semiconductor and IC technologies are ideal for copiers, banking terminals and other such scanning applications.