- Semiconductors & Devices
FOR IMMEDIATE RELEASE No. 3361
TOKYO, June 16, 2020 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today the launch of its N-series 1200V SiC-MOSFET (silicon-carbide metal-oxide-semiconductor field-effect transistor) featuring low power loss and high tolerance1 to self-turn-on. The new series will help to reduce the power consumption and miniaturize power supply systems requiring high-voltage conversion, such as electric vehicle (EV) on-board chargers, photovoltaic power systems and more. Sample shipments will start this July.
Mitsubishi Electric will exhibit its new N-series 1200V SiC-MOSFET at major trade shows, including PCIM Asia 2020 in Shanghai, China from November 16 to 18.
- 1Input capacitance/mirror capacitance (Ciss/Crss), as calculated by Mitsubishi Electric

N-series 1200V SiC-MOSFET
Product Features
- 1)Reduced power consumption and miniaturization of power-supply systems
- Junction field effect transistor (JFET) doping technology reduces both switching loss and on-resistance, achieving an industry-leading2 figure of merit (FOM3) of 1,450mΩ·nC. Power consumption in power-supply systems is reduced by approximately 85% compared to using conventional Si-IGBTs.
- By reducing mirror capacitance4, self-turn-on tolerance improves by 14 times compared with competitor's products. Thus, fast switching operation can be realized and helps reduce switching loss.
- Reduced switching-power loss enables the downsizing and simplification of cooling systems as well as the downsizing of peripheral components, such as reactor by driving the power semiconductor with a higher carrier frequency5, thereby helping to reduce the cost and size of overall power-supply systems.
- 2As of June 16, 2020 according to Mitsubishi Electric research
- 3Performance index of Power MOSFET, calculated by multiplying the on-resistance by the gate-drain charge (100°C junction temperature). Smaller values indicate better performance
- 4Stray capacitance between Gate and Drain existing in MOSFET structure (Crss)
- 5Frequency that determines the ON/OFF timing of the switching element in an inverter circuit
- 2)Six models for various applications including AEC-Q101 compliant models
- The product lineup includes models which are qualified with Automotive Electronics Council's AEC-Q101 standards. Therefore, the N-series SiC-MOSFET can be used not only in industrial applications such as photovoltaic systems, it can also be used in EV on-board chargers.
Sales Schedule
| Product | Standards | Model | VDS | RDS(on)_typ. | IDmax@25°C | Package | Sample availability |
|---|---|---|---|---|---|---|---|
| SiC-MOSFET | AEC-Q101 | BM080N120SJ | 1200V | 80mΩ | 38A | TO-247-3 | July 2020 |
| BM040N120SJ | 40mΩ | 68A | |||||
| BM022N120SJ | 22mΩ | 102A | |||||
| — | BM080N120S | 80mΩ | 38A | ||||
| BM040N120S | 40mΩ | 68A | |||||
| BM022N120S | 22mΩ | 102A |
Inquiry
Media contact
Customer Inquiries
Related articles
- Semiconductors & Devices