Electronic Devices
A traction inverter incorporating large-capacity hybrid SiC power modules mounted on a railcar has demonstrated its energy saving effect in commercial operation.
R&D category | Transportation |
---|---|
Purpose, feature or effect of the R&D | Envlronmental Measure, Energy Savings, Small Package |
Mitsubishi Electric has developed a large-capacity hybrid SiC*1 power module, and has commercialized a railcar traction inverter that incorporates these power modules as a world-first achievement.
A railcar equipped with the inverter has been in commercial operation since February 2012, and it has demonstrated for the first time in the world*2 the energy saving effect that can be achieved with SiC power modules.
A large-capacity power module with a rating of 1200A/1700V was developed by configuring a hybrid structure that combines SiC-SBD*3 and Si-IGBT*4.
This hybrid SiC power module records the world's largest capacity*5 in the category of IGBT module that incorporates SiC-SBD.
Railcar traction inverter incorporating a SiC power module
By incorporating large-capacity SiC power modules, power loss can be reduced to 30% of conventional inverters.
The SiC inverter is also 40% smaller and lighter than conventional inverters.
Tokyo Metro Ginza Line 01 series railcar that was used in the demonstration test for energy conservation
The SiC inverter was put in operation in February 2012 onboard a commercially operating Tokyo Metro Ginza Line 01 series railcar. In a field test, a 38.6% reduction in energy use*6 was demonstrated in comparison with conventional inverters in other railcars operating on the same Ginza line.
Moreover, with an increase in regenerative ratio to 51.0%, higher energy utilization efficiency has been achieved than ever before.
This was the world's first demonstration of the energy saving effect of a railcar traction inverter incorporating SiC power modules using a commercially operating railcar.
The above development utilizes, in part, the results of a study conducted under contract from New Energy and Industrial Technology Development Organization (NEDO) of Japan.